Hi,
I am trying to read cell voltage and temperature using BQ79656 for a single device.
Cell voltage reading is successful but reading temp via NTC connected GPIO is not working. Can anyone help me out or guide me what i am doing wrong.
This is cmd i am sending. CRC is also calculated and send
1) Wake is successful by sending wake Ping
2) {0xD0,0x03,0x4c,0x00} - OTP Ecc Test
3) {0xD0,0x03,0x09,0x01} - Array Address
4) {0xD0,0x03,0x06,0x00} - Direction Set
5) {0xD0,0x03,0x08,0x02} - Array Stack device
6) {0x90,0x00,0x03,0x08,0x01} - Top of stack
7) {0xc0,0x03,0x4c,0x00} - Read
8) {0xD0,0x00,0x03,0x0A} - Active cell 16
9) {0xD0,0x00,0x07,0x02} - ADC config 1
10) {0xD0,0x03,0x0F,0x0E} - ADC control1
11) {0xC0,0x05,0x68,0x1F} - Read cell voltage (successful)
12) {0xD0,0x03,0x0A,0x01} - Tref enable
13) {0xD0,0x00,0x0E,0x02} - Gpio Enable
14) {0xC0,0x05,0x8C,0x01} - Tref read (successful)
15) {0xC0,0x05,0x8E,0x01} - GPIO read
response for GPIO read in 0x8000 which is in active gpio, but step 13 its enabled.
Thank you