This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: Questions of BQ25750

Part Number: BQ25750
Other Parts Discussed in Thread: BQ25756

Dear Team,

Does BQ25750 can meet the spec or replace LTC4013? if no, please suggest suitable solution. Thanks.

Vin: 60V~80V Vout: 54V

For: Li-Ion battery

Many Thanks,

Jimmy

  • Hello Jimmy,

    The absolute max rating of VIN is -0.3V to 80V

    The recommend VIN is 4.2V to 70V. The BQ25756 will stop switching when VIN reaches VAC_INT_OV which is 74V.

    Best Regards,
    Ethan Galloway