This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56837: Heat sink

Part Number: TPS56837

We used the TPS56837 IC for 5V output in our design. Is this IC need heatsink ? 

  • Hello Viola,

    I don't think necessary. TPS56837 has good thermal performance. You can use webench thermal simulation.

    24Vin-5Vout-8A-500kHz-25C Ta, see below estimated Tj, about 79.54℃.

  • In our design we have to use this TPS56837 DC - DC Buck convertor. The Input voltage is 12V and the output Voltage is 5V with 8A current.  I simulate the circuit in we bench  designer, from the results the total power dissipation is 2.994W.  And I check the thermal stress for the IC @25 C its getting 152.59% of thermal stress. I need clarification on this issue.  Whether heat sink is required or not.

  • Hello Viola,

    It really depends on your application conditions (what's your ambient temperature? If high, maybe need to add heat sink; how many layers of your PCB board, does your board have good thermal dissipation performance?) and your thermal requirement (e.g. IC temp lower than 80C?).

    I simulated 12Vin-5Vout-8A-500kHz-25C Ta, webench estimated IC temperature is 75C. May I know how your '52.59% of thermal stress' come from?

    Our device max Tj is 150C. It has thermal shutdown protection when Tj beyond 165C.