Hi Brigitte & TI Team,
We are facing an LM5176 IC damaging issue while testing above 5A load with input voltage 33V & 30V output voltage.
Issue Details are as below:
We used the same values as mentioned in the LM5176 evaluation board, only updated feedback resistance so that the output voltage would be 30V.
It was working well for VIN 33V, and Vout 30V till 5A load. But above 5A load LM5176 IC getting damaging i.e system stopped working, output voltage not getting 30V ( only showing 4 or 3 V).
Note:
After analysis, it is observed that the impedance between Boot1 & SW1 is very low ( ~ 100 Ohm) & sometime high side mosfet (which is connected to HDRV1, SW1 & Boot1) also gets damaged.
This high side mOSFET has 60V max operating VDS voltage.
As of now, there are 5-6 qty LM5176 were damaged in the same manner.
We need your quick support on the same.