This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: Maximum LED Current?

Part Number: TPS61169

We are trying to drive some higher current UV LEDs.  Based on the data sheet, with a sense resistor of 0.58 ohms we should be getting 352mA

However when measured it is more like 150 mA max.  

It appears that there is too much noise on the sense resistor?  

Suggestions to try and fix the problem?