Other Parts Discussed in Thread: TPS40210
Hi team
My customer is using TPS40210-Q1 as fly-back to power IGBT drive.
One quick question about soft-start , when start up the SW will start to switch pulse skip sometimes as below:
Vin is 16V, Vfb is 5V; F=125kHz
abnormal waveform:
yellow:GDRV ;Green:Vsense; Blue:VDD; Purple :Vfb(5V)
As you can seen when start up, the switch frequency is not stable at 125kHz.(will skip pulse )
I've check there is no overcurrent when start up, Vsense max is 90mV
normal waveform:
yellow:GDRV ;Green:Vsense; Blue:VDD; Purple :Vfb(5V)
As you can seen when start up, the switch frequency is stable at 125kHz.(no skip pulse )
May I ask what reason may cause this kind of skip pulse?
Also does VSEE in datasheet is one of the IN+ of TPS40210 internal error amplifier ?
Looking forward for your response.
irene