Hi Experts,
My customer reported an issue of TPS65130 circuit: occasionally the negative output cannot start up.
The circuit is typical ckt in datasheet. It generate +/-12V output from +5V input. The load current is +/-20mA (MAX). Most of time the circuit working properly, but with a very low opportunity the negative output is always 0V, at the same time the possitive output is allways correct +12V. They observed the negative inductor current waveform during start up with questioned circuit. It shows the circuit trying to start up negative output however after a while the negative DC/DC stopped switching. The inductor current reach to arround 1A peak before it stopped. It cannot try again once stopped. It is confirmed it is not due to UVLO or thermal protection since the possitive output is always correct. And the device is not damaged since it can resume work some other time or change another inductor. I cannot find any other protection feature can result such kind of phenominen.
Attached is the start up waveform with: possitive o
utput, negative output , and inductor (negative) current.
Thank you,
John