Other Parts Discussed in Thread: LM5175, LM5175EVM-HD
Hello,
I have copied more or less the EVM. It works quite well, but it loads 110-120mA from a 7-8V input while is no load on its output. The circuit output is set to 12V so it works in Boost mode.
The used coil on first trial XGL1712-153, later changed to XGL1712-472, but nothing changed on load current.
Attached the schematic of LM5176, and the power part.
Attached oscilloscope picture of the shunt and LO2 gate, also LO2 and HO2 gate too.
The circled parts are not populated for now, but later would be added to reduce ripples.
Any idea is welcome.
Thank You in advance !
Zoltan