Hi
I have a query need your help.
The FUSE pin is directly connected to GND, when used on the client, the cell voltage is about 14.7V, and the communication is normal. However, after disconnecting the communication between the host system and gauge about 20s, no output voltage. After connecting to the system communication, FUSE is still set, then reset and clear the FUSE, the output is normal; after repeatedly disconnecting the communication between the host system and gauge for 20 seconds, there is still no output.
After pulling the FUSE pin to ground through the pull-down resistor 270K, the above symptoms do not occur.
Why does this issue occur after direct grounding? This problem can be solved by connecting a resistor of more than 200K in series to the ground.
Waiting for your reply.
Thanks
Star