Hi,
I am designing a custom board with BQ25672.
Can anyone review my schematics and provide valuable comments. Also, I have few questoion:
- our power supply specification is 12V, 2.5A. System load is 10W and we are using 2s,2P battery with 6.7Ah rating. Is input 2.5A is sufficient for our application considering battery charge current of 1A?
- What is the switchover time when VBUS input is gone and battery voltage comes into play to provide sys power?
- Current rating of BATFET?
Amit