This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005-Q1: Question about switching waveforms.

Part Number: LM76005-Q1

Hi

If you look at the switching waveform, there is a duty change in the middle.
So I tried both pfm/pwm modes and they were the same.
Normal waveform?

And in PWM mode, inductor heat was generated, but when I changed to PFM mode, the heat decreased. Can you explain why?

Thanks

  • Hello David,

    No, not normal, can you please share schematic and specification you design to.  Thanks.

    David.

  • Hi David

    Please refer to below.

    -spec-

    Input: DC12V~36V

    Output: 8.37V 2A

    Thanks

  • Hello David,

    The waveform's provided suggest your loop is unstable.  Looking at your frequency selection, you have 440kHz, calculating the ripple current in the inductor, you have a peak to peak current of 0.5A.  For a 5A output current device employing peak current mode control, this appears to be too low.  Suggest changing the inductor to 4.7uH and see if that helps. 

    Another thing to look at is your input filter.  You will need a 47uF cap at the input with and ESR of 0.3ohm to dampen, please try each of these things to stabilize the loop. 

    Hope this helps.

    David.