Hi Team,
My customer is looking for a budgetary estimate for a DC to DC converter circuit for their printer system.
The input will be LiON batteries.
The output needs to support 24 volts.
The highest option would be 20A out.
They can also look at the cost savings for 15A out.
The input needs to be 480W / efficiency / 50W per cell.
What that means is that if they need 480W and the circuit is 90% and each cell can deliver 50W,
they would need at least 10.6 cells.
The max pack voltage can be selected by them.
6S-2P would be a battery with a max voltage of 25.2 volts and it could deliver 30 Amps.
I'm not sure if that is a low cost configuration.
Maybe 5S-2P would be a lower cost circuit.
With a low voltage cutoff of 3.5V per cell, the input range would be 17.5 to 21V
and the cells can support 15A x 2 = 30A.
So on the low end 17.5V * 30A * 90% eff = 472W
Could you please kindly provide guidance base on the specs above?