Hello,
I am designing the circuit used TPS1H200A-Q1.
This TPS1H200A-Q1 is planned to be used in HOLD MODE.
When used in HOLD MODE, if the output current becomes larger than the current setting value, it will be clamped at the setting value and current output will continue.
If the junction temperature exceeds 175℃ due to continuous current output, a thermal shutdown will occur in the TPS1H200A-Q1.
Is there a risk that the TPS1H200A-Q1 will deteriorate if thermal shutdown occurs repeatedly?
I will be using TPS1H200A-Q1 with heat countermeasures by adding heat dissipation fins and heat dissipation patterns, but please be sure to confirm whether there is any risk of deterioration.
Regards,
MESH