Other Parts Discussed in Thread: TPS25772-Q1
Hello Ti,
I did not see register map in datasheet or in website.
Can you please share it with me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ti,
I did not see register map in datasheet or in website.
Can you please share it with me?
Hello Seong,
I want to use it with microcontroller.
I want to change rated power value while a usb device connected or not connected to type c port.
Also I want to see which values can share TPS25762-Q1 with microcontroller.
Hello Yunus,
By changing the rated power, do you mean changing the TX source capability? If so, you are unable to update these parameters on the fly while the device is operating. The TX source cap can only be preconfigured in the patch bundle's application configuration that is loaded when the device first boots.
For telemetry diagnostic information, I am able to share the register information here.
Hope this helps,
Seong
Thanks you for information. I want to clarify what TPS25762-Q1 can do.
I want to use 2 microcontroller and 2 TPS25762-Q1 on different equipment.
Type-C Output max will be 20V 3.35A 67W.
I want to do power management between these USB Type-C outputs.
Can you please answer questions below?
1. Are there any I2C command to close the output pmosfets with TPS25762-Q1?
2. Can microcontroller reduce the output current capabilities of TPS25762-Q1 over I2C while a usb sink device connected to USB Type-C sinking some current. For example,
3. Can microcontroller reduce the output current capabilities of TPS25762-Q1 over I2C while a usb sink device not connected to USB Type-C. For example,
4. Is there any other way to reduce sinking current of the connected usb device?
Hi Yunus,
Are you familiar with our dual-port solution, TPS25772-Q1? This device also has an integrated source power policy management system but it can automatically (as configured) manage power sharing between two ports.
FYI - the TPS25762-Q1 supports up to 65-W USB PD power.
To answer your questions:
Is there any reason why you would want to charge a Sink device with less power?
Are you aware that you can configure up to 7 PDOs/APDOS?
BR,
Seong
Hi Seong,
Thanks you for your kindly respond.
Yes I know TPS25772-Q1. But TPS25762-Q1 and the other TPS25762-Q1 will not be in the same board, so TPS25772-Q1 is not an option from this view.
There is a reason that the total power of the two equipment will be limited. There will be a power management between equipments.
Is there any reason why you would want to charge a Sink device with less power?
Can you offer another solution for such design?
I can share more information about our projects in a meeting.
I want to discuss with an online meeting. Is it possible?
Hello Yunus,
I will close this thread and send you an E2E friendship request. Let's continue our discussion via DM.
BR,
Seong