ADCDATA 1-8 registers return 0x0000 when read
- attempting to use the ADC1 register to read voltage divider data with a NTC thermistor to determine gate temperatures.
The documentation says there are 3 possible sources of error, see below. I'm using the internal vref and I can measure it as 4.0 volts on the Vref output pin. Any suggestions as to how I might check the other two error conditions?