Other Parts Discussed in Thread: UCC28730
Hello,
Regarding the controller UCC28730-Q1, I have another 2 concerns:
1. In order to keep the stability in all the operating range, it is indicated the next equation of Cout (Ecuation 22 of datasheet):
My question is: Is fMAX the maximum indicated at datasheet (83.3kHz), or can be 28kHz (minimum switching frequency of the controller)?
2. In our design, we are using the Auxiliary winding to also supply some loads (150mA).
In this scenario, how it impact on the ecuation that determines the output capacitance? The same ecuation for each rail?