Other Parts Discussed in Thread: CSD18513Q5A, LM5145
I cannot understand why there is the need to used different mosfets for the high and low side.
1. All application examples and webench configurations use different but very similar Mosfets on the low and high side, why is this?
2. For BOM consolidation and cost I would like to use the CSD18513Q5A for both high and low side switches, is this ok?
Part will be used for two applications:
9-22V Input, 3.3V 15A Output
9-22V Input, 5V 20A Output