I'm looking for some ideas on designing a cheap/compact method to limit the maximum charge and discharge current of a single battery cell.
Requirements are voltage approx 1.5 to 4.0 V, current limiting to 1A; on over current, do not shut off but limit max current to 1A.
I am in the process of designing this using two TPS25221 placed back to back, but I'm not sure if this part would be happy in a constant overcurrent situation because of the heat dissipation. I'd rather use a switching CC regulator for this.
Is there a single part that can perform this task bidirectional? If not, what part would be a good choice for switching current limitation, would a switching LED driver be a viable alternative?
Thank you,