This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59108F: ON/OFF and PWM configuration doesn't works

Part Number: TLC59108F
Other Parts Discussed in Thread: TLC59108

Hi,

I am trying to use the TLC59108F device. The device reply to me well and I don't understand why it doesn't works.

In particolar, I configure the device by set normal mode into MODE1 register. 

After that, I put all the LEDs in OFF mode by using LEDOUT0 and LEDOUT1.

After that, every 500ms I swit1253ch the LED1, LED2 and LED3 to full ON and then OFF.

If I put a LED in PWM mode, it works only if I put 0 or 255 into the register, otherwise it remains always on.

Where is the error?!?

Thanks

Marco