We have a LP8764-Q1 based design. The GPIO4 is used as an enable input and there is no pull up selected for this input.
VCCA,PVIN_B1,PVIN_B2,PVIB_B3,PVIN_B4 = 5.0V
VIO = 3,.3V
We read VOUT_LDO = 1.8V
The actual design has 100K pullup on GPIO4. So instead of reading 3.3V @ the GPIO4, the node was reading 2.2V
I removed the 100K pull up resistor to 3.3V and we still do read 2.2V @ GPIO4.
This was a working board and this board has gone through temperature stress test.
The part is working intermittently. When the board is subjected to vibration via tapping the board, the PMIC turns off output
Trying to understand what could be going on. Should we remove this part and send it for failure analysis ?