Other Parts Discussed in Thread: BQ25730, , TPS25751
Hi,
We use the couple TPS25750 + BQ25730 to manage a product on battery. In order to save as much power as we can when our device is powered off, we try to disable the OTG supply in our BQ by using the register bit EN_OTG. When shutting down the device, we set this bit to 0. But I noticed if we plug a USB drive on our device, it seems to be enabled again. We monitor our battery current, and it's going up to the same level as when OTG is active. We suspect the TPS to automatically enable the OTG bit when something is plugged.
We would like to know if there is a way to prevent the TPS to auto enable OTG, until we allow it again ?
Or, second option for us, would it be possible for the TPS25750 to automatically disable the OTG when the USB drive is unplugged (because our system will be powered off so our processor unit cannot react to the "unplugged" event the TPS fires) ?
That second choice is not the best, but at least if a USB drive was plugged then removed while our device is off, it would fall down to a minimal consumption level again and save some battery.
Thanks and regards,
Richard