This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563231: Recommended inductance value at 3.8V output

Part Number: TPS563231

Dear Specialists,

My customer is considering TPS563231 and has a question.

I would be grateful if you could advise.

---

・We are planning to use a 3.6uH inductance for 3.8V output.

If 3.6uH is not appropriate, please let me know the appropriate value.
・Input voltage: 5V
・Output voltage: 3.8V
・Output current: 1.6Amax

The inductance value listed in the data sheet,
3.3V output (2.2uHmin/3.3uHtyp/4.7uHmax)
5V output (3.3uHmin/4.7uHtyp/4.7uHmax).

Since 3.8V is within this range, we think 3.6μH is not a problem.

We'd like to confirm just in case

---

I appreciate your great help in advance.

Best regards,

Shinichi