This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5163-Q1: Leakage of PGOOD ports in LM5163-Q1 (and LMR38010-Q1)

Part Number: LM5163-Q1
Other Parts Discussed in Thread: LMR38010-Q1,

Good morning

What is the maximum input leakage @150°C (or 125°C) of PGOOD port

(i.e. when voltage is regulated inside of the ‘good’ range,
it should be a MOS --> Zero Gate Voltage Drain Current)

for:

  • LMR38010-Q1
  • LM5163-Q1

@Vds = 5V - 10V

Do you have any data or graph showing this aspect?

If you don’t have any,
can you suggest similar discrete MOSFETs to draw data from?

Thank you very much in advance
Best regards