Other Parts Discussed in Thread: TPS3703
Hi,
I'm looking for an overvoltage/undervoltage detection IC.
・Detection power line: +12V, +5V, -12V
I selected TPS3700 x2 as the 12V/-12V line monitoring IC and TPS3703 as the 5V line monitoring IC from the TI website.
Q1. Has TI released an IC that can monitor all three systems (+12V, +5V, -12V) at one chip? Alternatively, an IC that can monitor two systems (+12V, -12V) at one chip is fine.
Q2. If you have any recommended monitoring ICs other than the above devices, please let me know. It would be good if it could detect overvoltage/undervoltage on the power line.
Thanks,
Conor