Hello expert,
May I know the A and non-A version difference on DBV package? I know the difference on PK package is IN or GND pin. But I'm not quite sure on DBV, could you help?
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert,
May I know the A and non-A version difference on DBV package? I know the difference on PK package is IN or GND pin. But I'm not quite sure on DBV, could you help?
Best regards,
Ann Lien
Hey Ann Lien,
Thank you for your question! All the DBV (SOT-23) TLV709 have an A there is not non-A version of the DBV (SOT-23) package. This doesn't have any associated meaning like with the PK packages. So all DBV (SOT-23) packages are the same other than the voltage rating which is denoting by the following:
TLV709AxxDBVR (SOT-23), xx = voltage rating, 01 = adjustable version, 33 = 3.3V version, 50 = 5.0V
This information is usually found towards the end of the datasheet and for the TLV709 section 8.1.2 Device Nomenclature.
Thanks,
McKyla