Like IMVPs, I would like to change the current flow from 0-600amps depending on the input voltages. My requirements are to have a mosfet with very low value of Rds within a maximum range, which helps with providing high current for a range of input voltages.
Need some guidance with a topology of mosfets in parallel to achieve this functionality. The idea is to have a set of parallel mosfets to work for 0-200amps range and by a combination with another set for 200-400amps range and so on.