This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409EVAL: About the schematic design of LM3409, output 5V related issues

Part Number: LM3409EVAL
Other Parts Discussed in Thread: LM3409

For schematic design of LM3409, such as PDF document design, if the input is 24V and the output is 5V, how should the corresponding parameters be designed? Does VTURN-ON need to be configured?

  • Hi Songhao,

    • Please first set up your design specification - like Vin, Vou, frequency, Iled and so on, then follow the design steps in this application note.
    • The VTURN-ON depends on your application, you can change it accordingly.

    Many thanks!

    BR,

    Hailee.