I am using TPS65265 with Vin=12V to get triple output voltage of 3.3V, 5V and 3.7V. Help me in choosing DC-DC loop compensation values for each of the output channel. schematic of same is attached.TPS65265.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using TPS65265 with Vin=12V to get triple output voltage of 3.3V, 5V and 3.7V. Help me in choosing DC-DC loop compensation values for each of the output channel. schematic of same is attached.TPS65265.pdf
Hi,
I think is as same as below link. Because you use the same schematic. I have responded to below thread and will close this one. Thanks.
Aurora
Hi,
The above link says Page not found. Please share link once again.
Regards,
Radhika
Hi Radhika,
For inductors and compensations, my suggestions are shown below:
1. Change R23 to 21kohm (customers can choose similar values);
2. Change R29 to 16.4kohm, change C54 to 4.7nF;
3. Change R33 to 12kohm, change C60 to 6.8nF;
4. Change L3 to 5.6uH or 6.8uH;
5. Change L4 to 6.8uH or 8.2uH.
No other obvious problems. Thanks.
Aurora