On page 9 of the datasheet from June 2023 in chapter 7.6 the safety-related certificates are missing. When will this be added, especially according to DIN EN IEC 60747-17 (VDE 0884-17)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
On page 9 of the datasheet from June 2023 in chapter 7.6 the safety-related certificates are missing. When will this be added, especially according to DIN EN IEC 60747-17 (VDE 0884-17)?
Daniel,
The UCC14141-Q1 is in progress for achieving IEC 60747-17 (VDE 0884-17) and the expected date of completion is Q32024, likely end of September. Other mentioned certifications from section 7.6 are UL1577 which is now complete and CQC GB4943.1 which is nearing completion and expected by end of Q12024. Unfortunately VDE has the longest queue for completing their required certification testing.
Regards,
Steve