Hi,
I'm just testing a new dc/dc converter design using a LM5164DDAR. At some loads there is an audible noise from the inductor and also a change in the ripple. This is my schematic, I'm using a shielded inductor from Sumida CDRH127/LDNP-560MC for L1
With a load of 24 ohms and a duty cycle of 69% (f = 20 kHz) the ripple looks like this and there is a audible noise from the inductor.
With a load of 24 ohms and a duty cycle of 98% (20 kHz) the ripple looks like this and there is no audible noise.
I've increased the capacity of the input and output capacitors but the noise doesn't change.
Do you have an idea what I may change?
Thanks in advance.
Kind regards,
Roger