Dear TI support team,
I am working on a design including the BQ51003 as a wireless receiver. For some reason the charging is interrupted occasionally, so I am currently trying to identify the root-cause for it.
When investigating the on-board signals that potentially could trigger a shutdown of the output voltage, I observed that the voltages at the FOD and ILIM pins seem to be highly affected by shielding different areas of my PCB. To do so, I have added an additional ferrite sheet between the receiver coil and the PCB and moved the PCB slowly in different directions. The receiver coil was always centred underneath the ferrite sheet during that test.
What I see is that the AC component of the signals changes significantly and also that the likelihood of the power transfer to be interrupted changes. The yellow waveform at CH1 represents the signal at the FOD pin and the red waveform at CH2 represents the signal at the ILIM pin. Unfortunately, I could not find the waveforms for these two pins in the datasheet to compare them to my measurement results, so I would kindly ask for your support to evaluate them. Is there even an AC component to be expected for these two signals or does it result from the magnetic field coupling into the signals? Also, what are the precise thresholds for these two pins to trigger the shutdown of the output voltage?
I observed that the solution to the right leads to the best test results in terms of continuous charging. Is that to be expected for the corresponding waveforms?
Please let me know if any additional information is required by you to support in this regards.
Thank you and I am looking forward to your reply!
Best regards,
Leonhard