Other Parts Discussed in Thread: BQ76200, BQ76930
Hi
The customer design with BQ78350, BQ76930 and BQ76200. It was found that the static self-consumption is very large, around 0.4mA.
After the battery capacity was full discharged, it entered Shutdown (voltage lower than 1.75V) mode after being stored for about one month, which made the battery unusable.
It needed to be disassembled to charge the battery to wakeup the board.
How to configure parameters to reduce power consumption?
Waiting for your reply.
Thanks
Star