I am designing a new PCB with a number of different rails:
I need to use the LP8764 in 3 different configs:
Quad phase (1 output) :20A
3 phase, 1 phase 15A, 5A
2phase, 2 phase 10A, 10A
Regarging the orderable parts, which is the best to obtain as a starting point. I have evaluated the reprogramming of the NVM using the EVK (LP87444Q1EVM). I have been able to change this from 1,1,1,1 to 4 phase mode.
Please confirm the recommended blank part to purchase:
LP876411B4RQKRQ1
LP876411B5RQKRQ1
LP876441B1RQKRQ1
Also confirm if any of these parts are locked. I would like to be able to customise them over I2C as needed, with a known I2C address.
Thanks,
Alleyn