Other Parts Discussed in Thread: BQ24296
Hi,
I am using the BQ24297 single-cell charging IC for my product.
I am facing an issue regarding the incorrect detection of the VBUS.
I have connected a 5V, 3Amp adapter to the VBUS pin, but when I read the Charger Status Register, it shows VBUS:1 (USB host). As a result, my IC limits the charging current to the battery.
Note: I am not updating any parameters to the IC, so it will use default parameters during power-on.
Below is the schematic I have attached for reference.