Other Parts Discussed in Thread: GAUGEPARCAL,
Hello
For an 8S family of battery packs I have just provided data to GAUGEPARCAL and obtained a set of parameters as follow:
EMF 3802
EDVC0 519
EDVC1 0
EDVR1 1
EDVR0 439
EDVT0 1
EDVTC 11
They have been obtained evaluating an 8S2P pack, but we also need to program them in the data flash of bq78350R2 gauges for 3 differnt type of packs: 8S1P, 8S2P, 8S3P.
The parameter file obtained from GPC says:
CEDV parameters resulting from the fit. If EDVV bit is set to 1, EMF and EDVR0 have to be multiplied by the number of serial cells when written to data flash
EDVV does not exists in 78350, I think this gauge by default has all paramters scaled at cell level, is it correct ?
How do I program EMF and EDVR0 in the DF, considering that they have been calculated on a 8S2P pack and I need to program also to 8S1P and 8S3P :
- just multiply by the series cells ?
- or I have to scale also by the parallel cells, and in which case how exactly ?
Thanks in advance
Pietro