Other Parts Discussed in Thread: TPS61094, TPS61299EVM-016, TPS61299, TPS61299EVM-103
Hi,
We designed a product that uses the TPS61021A to power a modem.
Recently we tested the PSM (Power Saving Mode) of the modem that requires the modem to be powered with a current as low as 4µA.
We measured the current actually drawn, and we observed a 100µA average with picks of around 100mA.
I saw that the chart is not showing below 100µA (our Vout is 3V3 and Vin between 3V and 2V):
I saw a similar problem here:
TPS61021A: Pulsed Currents on Demo Board - Power management forum - Power management - TI E2E support forums
Is it still expected to have this behaviour like said in the link above or is it not a normal behaviour.
if it is an expected behaviour, is there a way to reduce the consumption with a light load ?
if it is not possible to reduce greatly this consumption, could you recommend a better component that can handle high currents during a network connection (up to 1,5A) and low currents during PSM ?
Thank you beforehand,