This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV803E: Glitch pulse during power up

Part Number: TLV803E
Other Parts Discussed in Thread: TLV803, TLV809

Hi, TLV803/E support team

In the TLV803 datasheet, the glitch pulse during power up is shown as below. I can see it in the PSpice simulation result.

I think that this unexpected glitch pulse is appeared not only the open-drain device (TLV803/E) but also push-pull device (TLV809/E). Is this correct?

Are there a way to improve this glitch pulse? For example, adding external parts or changing device

Regards,

Tamio