Other Parts Discussed in Thread: TPS54200, TPS92201
Hello,
On page 26 of the docs there is an example schematic - Figure 8-26. 5-VIN, 1-A, 1-piece IR LED, Analog Dimming Reference Design
A) Are there any components that would need changing in this schematic increase the output to 1.5A; apart from changing the sensing resistor to 66mohms?
B) Are there any components that would need changing in the schematic to allow a 12v input rather than the described 5 V ±10% VIN? I don't think there are but it is unclear to me why the docs don't describe a wider VIN in the table
Many thanks,
Sam