Other Parts Discussed in Thread: LMG2610
Hello, can multiple LMG1210s be ganged in parallel for higher current?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff,
Thanks for reaching out.
We would not recommend driving gate drivers in parallel. This is due to the possibility of an output mismatch on the combined gate drive signal.
Is there a requirement in which a singular gate driver would not work such as needing quicker rise and fall times?
Thanks,
Jeremiah
Hi JSR,
Could you please provide more information about your application such as power level, topology, input voltage, and output voltage?
Thanks.
Hi Jeff,
As outlined in Section 8.3.1 of the LMG2610 datasheet, the LMG2610 GaN power FETs are intended to be turned on in either zero-voltage switching (ZVS) or discontinuous-conduction mode (DCM) switching conditions. Regarding device compatibility, if the buck converter can be operated in a manner to abide by the conditions listed above, it would be suitable for the application. Otherwise, this device, currently cannot support hard-switching applications.
Best Regards,
John