This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS389006-Q1: TPS389006004 I2C ADDR Setting Resistor

Part Number: TPS389006-Q1

Hi TI,

Can we use 47K ohm resistor for I2C addr 0x34?

On datasheet, TI recommend 47.5kOhm but I think 47Kohm can use as well.

Because it is close to 47.5K rather than 37.4K and 58K.

Best regards,