Other Parts Discussed in Thread: TM4C123GH6PM, BQ34Z100,
I have a battery pack of Lithium Ion cells of capacity 41.6 Ah (Charging Voltage = 16.8V) (Nominal Voltage = 14.52V)(Charging Current = 10A)(Discharging Current = 12.5A). I want to measure its capacity and want to display it on screen with the help of micro-controller TM4C123GH6PM. IC should communicate through I2C. I have found "BQ34Z100" IC for this. It is "Wide Range Fuel Gauge with Impedance Track Technology". In datasheet, a line is written as " Supports battery capacities above 65 Ah" and "Supports charge and discharge currents above 32 A". Then i have searched for another part "BQ34Z100PWR-G1". In it "Supports battery capacities up to 29 Ah with standard configuration options" is written with "Supports charge and discharge currents up to 32 A with standard configuration options". But, i did not find any IC part that support battery capacity what i need. So, can i use "BQ34Z100EVM" for my application. If not then please suggest me any other IC part that fulfill my requirement.
Thanks & Regards
Shashi