Other Parts Discussed in Thread: TPS65987D, BQ25723, , BQ25798
Hi
The customer design a charging circuit with TPS65987D+BQ25723, but this combination could not use an external LED light to indicate the charging status.
The original design is to use TPS65987D to obtain PD protocol power supply, and then the I2C of 987D configures BQ25723 charging voltage/current
The design conditions are: controlled by 987D, the maximum power supply to BQ is 20V/3A, the minimum is 5V/1A; the battery charging voltage is 8.7V, and the maximum charging current is 5A.
Now under the same condition of using the 987D fast charging protocol chip,
They want to replace BQ25723 with BQ25792 and use VIN2 of 792 as input. Can it replaced?
Or are there any other recommendations for buck-boost chips with STAT status output?
Waiting for your reply.
Thanks
Star