Currently design a transimpedance amplifier system with multiple op amps operating under dual supply conditions. I was looking into using a TL7660 to convert a 3 V input supply to a -3V so that I can supply both 3 V (Vcc) and -3 V (Vee) to my op amps supply rails using a single output channel from my power supply.
Albeit a simple circuit, I want to draw out a schematic with TINA TI using the TL7660 SPICE model to visualize how the circuit may look (and simplify its transition to a PCB using Altium). There is only a PSPICE model available on the product page.
I am aware that this may not be a "useful/complicated" enough component to have a SPICE model for TINA TI but thought it wouldn't hurt to ask.
Apologies for any inconvenience.
Best,
Cam