Other Parts Discussed in Thread: LM5171
Hi team,
My customer has two questions about LM5170-Q1 EVM.
1. User guide mentioned, under buck mode, need to turn on starting from HV-PS -> LV-PS and then LV E-load. May I know what's the reason why connecting LV-PS? Since buck mode should be coming from HV-PS. Also another thing mentioned in the user guide in figure3., if the output voltage loop is closed, the LV-PS can be disconnected in buck mode operation, what does output voltage loop mean?
2. Also customer running actual testing, customer didn't turn on LV-PS, but other setting same as userguide, (HV-PS -> LV-E-Load -> Apply Master Enable -> Apply an analog voltage gradually rising from 0V to 1.5V at ISETA) But LV output only has 8V(full load). Once the load becomes 1A, the LV output has rised up over 20V, not regulating at 12V, is this behavior expected?