Other Parts Discussed in Thread: LM5013
Hi,
I have designed a power board for my company using your LM5013-Q1. The board powers a rugged PC which we intend to sell as a premium product. I used your WEBENCH tool to help get a good design, or so I thought. Here´s the demands: Vin nom: +28V, max: +40V. Vout: +12.5V. Iout nom: 1A, max: 3.5A. Temp demands are -40°C to +65°C working environmental temp and -45°C to +80°C storage temp.
Our schematics for the circuit looks as follows:

The ferrite beads and the extra capacitor at the output connector is for meeting EMC demands. When we tested the complete assembled unit all seemed fine. We performed a burn-in test with no problems.
But when we put the units in our climate chamber for a cold test in -40°C more than one third of all units refused to start! Only after some time in room temperature with power on they slowly were able to power the motherboard enough to start the PC. I quickly found out that the power board were unable to output a correct voltage in cold climate. But not in every unit, only some...
We sprayed cold spray to different areas on the power board to try to identify the problem to any particular component but Vout was only affected when we sprayed the LM5013 IC. Nothing happened when we tried to concentrate the cold to surrounding components, only when cooling the LM5013.
I started thinking if we might have damaged the boards somehow in our previous testing, but I had a panel with 7 new "untouched" boards directly from our supplier. We tested each board in the new panel by connecting them on the test bench to DC power in and to our PC for power out and then spraying them with cold spray. Turns out that of 7 board one was showing bad tendencies, one was more ore less useless while the rest was better. So the bad behaviour was there from the beginning.
I scanned your web page for info on the LM5013 to see if there were something I might have missed or designed poorly. I found the " Stability Analysis and Design of COT Type-3 Ripple Circuit" which dealt with the stability of the circuit. I took the two bad boards and one OK board and hooked up my PicoScope to it. I used a resistive load of 8 ohm to load the output and started to test all about the boards.
I changed surrounding components testing different values but it wasn't until I changed the switching diode that things started to improve! The diode we had used was a VSSB310. It has an If (AV) of 3A and a Ifsm of 80A which I thought should be sufficient, but when I replaced it with a FSV12100V with If(AV) of 12A and Ifsm of 220A the board worked better. Now the board managed to keep the power up even at cold climate!
But why really? The LM5013 datasheet doesn't say that much about the switching diode and what parameters are the most important. What was it with our original diode that was insufficient? What parameter made the FSV12100V work? That's my first question.
Second question is about stability. It turned out that even when the units now managed to start up properly at -40°C it was only at the nominal Vin of +28V. If we lowered the Vin we still had problems... So now I looked at my oscilloscope curves and tried to understand how to improve the stability at lower Vin. We use the type-3 ripple injector circuit to minimize output ripple but it seems very sensitive to any miscalculations. For example, we use a 1.2nF capacitor although several examples in the datasheet use 3.3nF. I tried to change our 1.2nF to a 3.3nF but the result was a much higher dependency on the Vin. Vout now changed a lot more with different Vin so I had to change it back. Calculations gave that the capacitor that connects the ripple injector circuit with the FB pin should be bigger than 53pF so I changed it from 47pF to 68pF. That seemed to improve stability, at least at room temperature and at least in my oscilloscope measurements. Now I could turn down the Vin to about 14V without getting the "double pulses" that is a sign for instability, according to the application report SNVA874.
I came up with the following values for improved stability: R4: 220kohm, C25: 1,0 - 1,2nF, C26: 56 - 68pF. I also changed the R2 FB resistor from 475kohm to 470kohm to lower the Vout a bit. When we tested these values in some problem units they still had issues with Vin lower than +28V at -40°C. My changes didn't help at all!
Then I tried yet another switching diode. We had also bought a V8P12HM3_A/H which in my opinion has similar data as the FSV12100V. If(AV) is 8A, Ifsm: 140A and Vrrm: 120V. No big differences. But by just changing the diode the unit that demanded +28Vin to start in -40°C now willingly started at +16Vin! WHY?? Again, what parameters make the difference?? The V8P12 diode has a bit lower junction capacitance. Is that what helps here? I cannot understand this. Please help me!