Hello,
Qmax update rules.
1, The battery temperature is between 10-40℃;
2, One charge/discharge exceeds Qmax*37%;
3, Battery voltage is not in flat area.
Do the temperature rules have to be satisfied during charging/discharging as well?
For the scenario below (Rule 2 and Rule 3 are satisfied; Rule 1 is not satisfied during charging and is satisfied during Relax), is Qmax updated?