Hello:
The M483 new project plans to use LM36274YFFR, please check the schematic diagram. Thank you!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
The M483 new project plans to use LM36274YFFR, please check the schematic diagram. Thank you!!!
Hi Jimmy,
The customer connect LCM_EN1 and LCM_EN2 to ground, so they don't need the VSP and VSN?
BR
Patrick
Hi Patrick:
1、The customer planned to use I2C control to save GPIO, so it was grounded.
2、Please check the location of the backlight VIN, as shown in the picture, with RC filtering added? Could you please check if it is possible
3、In addition, The screen backlight specification is 6 series and 3 parallel, and the planned maximum backlight current is 20 mA per channel, totally 60 mA
The inductance specifications are as follows. Would you please check if they meet the requirements,Thanks!!!
Hi Patrick:
Please check about the location of the backlight VIN, as shown in the picture, RC filtering is added.
Could you please check if it is OK, Thanks!!!
Hi Jimmy,
I think the RC is ok, but it is better to follow the datasheet.
BR
Patrick