This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5451: Pull-up/down resistor value

Part Number: ISO5451


Hi team

Do we have a specific value of pull-up/down pin? Like IN+ and IN-.

BTW, should we add a RC filter between MCU and ISO5451? If so, do you have a recommended RC values? Thanks!

  • Hi Shaofeng, 

    I found this post that talks about PU/PD resistances :)

    It's recommend to add an RC filter if the trace is long from the MCU to the gate driver. I would recommend a ~100ohm resistor and a ~100pF capacitor as a starting point, and fine tune it to suit the system. 

    Thank you! 

    Vivian