I'm trying to use it with the VDD-VEE 18V setting,but it can be 17.5V due to resistance variation.
Can it be used at 17.5V without any problems?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to use it with the VDD-VEE 18V setting,but it can be 17.5V due to resistance variation.
Can it be used at 17.5V without any problems?
Hi,
If you design to achieve 18 V then ok as there can be some small variations due to resistor tolerance which you should use better tolerance resistor such as 1% grade or better than 1% to minimum the resistor tolerance caused variations to your design.