This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC14240-Q1: Can it be used at 17.5V without any problems?

Part Number: UCC14240-Q1

I'm trying to use it with the VDD-VEE 18V setting,but it can be 17.5V due to resistance variation.

Can it be used at 17.5V without any problems?